Configure the screen saver
The screen saver extends the life of the HMI device screen by dimming the brightness level when activity is not sensed for a specified amount of time. When the screen saver activates, the HMI device screen displays a moving image at a reduced brightness level. When activity is sensed, the screen saver deactivates and the screen brightness returns to the normal level.
To configure the screen saver
- On the HMI device or in theSystem Banner, selectNavigation
and then select Settings. - SelectDisplay. The Display popup opens.
- To enable the screen saver, selectTurn on Screen Saver.
- To configure the screen saver, change the following settings:
- Wait.To change the delay before the screen saver appears, selectWaitand enter the number of minutes. The default is 10 minutes.
- Brightness.To set the brightness of the screen saver, in the bottomBrightnessbox enter the number using the virtual numeric keypad or an external keyboard. The default is 10. 100 is the brightest.
- SelectClose
.
Provide Feedback