Configure Ethernet ports
Configure the link speed and duplex mode for the available Ethernet links of an HMI device:
To configure Ethernet ports
- On the HMI device or in theSystem Banner, selectNavigation
and then select Settings. . - SelectNetwork. TheNetworkpopup opens.
- Select theConfigure Ethernet Porttab
. - To to switch on/off LLDP Protocol support for 5510 HMI device, selectLLDP Protocol.TIP:PanelView5310 HMI devices do not support LLDP Protocol.
- To use two ports in the Ethernet configuration, selectEnable Ethernet Link 1andEnable Ethernet Link 2.TIP:Two Ethernet ports are available on thePanelView5510 HMI devices only.PanelView5310 HMI devices only interact withEthernet Link 1, and do not support DLR topology.
- Specify the network connection speed and how a port sends and receives data:
- Automatically.To automatically sense the link option and speed based on the network connection, selectAuto negotiate.
- Manually.To set the desired network connection speed for the ports, under the Ethernet link for one or both ports, select aLink speedoption and aLink duplexoption.
- SelectClose
.TIP:Tips:- 10 Mbpssets the network speed to10 megabits per second.
- 100 Mbpssets the network speed to 100 megabits per second.
- Half.Sends data or receives data, but not at the same time.
- Full.Sends and receives data at the same time.
Provide Feedback