Change the name of the HMI device
Each HMI device has a default name that identifies it to other devices on the network. Change this name using 15 characters including letters, numbers, and hyphens. The first character of an HMI device name must be an uppercase or lowercase letter.
Change the name of the HMI device
- On the HMI device or in theSystem Banner, selectNavigation
and then select Settings. - SelectHMI Device. TheHMI Devicepopup opens.
- In theHMI device namebox, enter the new name by selecting the keys on the virtual standard keyboard or using an external keyboard.
- SelectClose
.
Provide Feedback