Adjust screen brightness
Adjust the brightness of the HMI device screen by changing the backlight level.
To adjust screen brightness
- On the HMI device or in theSystem Banner, selectNavigation
and then select Settings. - SelectDisplay. TheDisplaypopup opens.
- In theBrightnessbox at the top of the screen, adjust the backlight level. Enter values between 1 and 100.TIP:At 1%, the display is minimally visible. The default 100% makes the screen fully bright.
- SelectClose
.
Provide Feedback