Lost connection to HMI device at address <x>
Possible cause and solution:
- The HMI device lost power or is disconnected from the network.Verify the HMI device is powered on and connected to the network.
- The workstation is busy processing requests from other programs, processes, or services.OpenTask Manageron your workstation to verify that no other program, process, or service is impacting the performance of the workstation.
Provide Feedback