HMI project file cannot be downloaded
Possible cause and solution:
- File downloads are disabled on the HMI device.Check theAllow download and Firmware updatesoption on theHMI device configurationscreen.
- Another file download is in process.Wait until the first download is complete and then try again.
Provide Feedback