Logged on as Guest user
Possible cause and solution:
- The Guest user is automatically logged on at system startup. When you log off the system, the Guest user account is automatically logged on. This is because only one user can be logged on at a time.To log on with assigned security access, log on using the correct user name and password or PIN. Contact the System Administrator for this information.
Provide Feedback