Cannot log on to application on HMI device
Possible cause and solution:
- When a login attempt fails and the current user or Guest remains logged on to the application on the HMI device, it may be because the user security account used to log on does not exist for the application. The user name and password or PIN used to log on may also be incorrect.Contact the administrator for the correct user name and password or PIN.
Provide Feedback