What does the red outline around a graphic element indicate?

Possible cause and solution:
  • The graphic element is in error. Errors occur if, for example, an invalid tag type cannot be written to a property of the graphic element, a tag bound to a property does not exist in the controllers referenced in the project, or an operation cannot be performed in a table.
    Tap the
    Error
    icon Icon: Runtime Error button on the graphic element or group to open the
    Error list
    . The graphic element or group fills with red and the error list opens. Scroll down through the errors for the graphic element to identify the issue. For a group of graphic elements in error, swipe right or left to display the errors for the next or previous graphic element that is in error within the group. After fixing the problem, the red outline and
    Error
    icon Icon: Runtime Error button disappear.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal