Graphic element does not change states

Possible cause and solution:
  • The state table does not exist.
    Create the state table on the
    Animations
    tab of the
    Properties
    window for the selected graphic element.
  • The state table containing the state changes is not selected in a
    State Previous
    or
    State Next
    command.
    Verify that the state table is selected for the
    State Previous
    or
    State Next
    commands on the
    Events
    tab of the
    Properties
    window for the selected graphic element.
  • The state change does not exist in the state table.
    Verify the values of the properties in the state table on the
    Animations
    tab of the
    Properties
    window for the selected graphic element. If the property does not appear in the state table, on the
    Animations
    tab, edit the state table and select the property.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal