X icon appears on graphic element

Possible cause and solution:
  • The graphic element is in error.
    Tap the
    Error
    icon Icon: Runtime Error button to open the
    Error list
    . Scroll down through the errors for the graphic element to identify issue. If there is a group of graphic elements in error, swipe right or left to display the next or previous graphic element in the group in error. After fixing the problem, the
    Error
    icon Icon: Runtime Error button disappears.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal