Data Log Warning icon appears in System Banner

Possible cause and solution:
  • A referenced tag does not exist in the controller.
    Check the configuration of the data log in
    View Designer
    . Export the data log to view tags with Bad Quality.
  • There is a communication issue with a controller.
    Check the controller path and the physical connection between the HMI device and the controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal