Data Log Error icon appears in System Banner

Possible cause and solution:
  • The data log service is stopped.
    Verify that the HMI device contains an SD card that is not missing, full, or read-only and then reboot the HMI device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal