Cannot export data to SD card
Possible cause and solution:
- The SD card as insufficient space.Insert an SD card that has enough space to contain the exported data log file.
- The SD card is not present.Verify that the SD card is inserted into the HMI device.
- The SD card is read-only.Insert an SD card that has write permissions.
- The SD card is not a supported type.Insert a supported SD card.
- The SD card is not the supported format.Insert an SD card that has a supported format of either FAT32 or EXT3
- The SD card is corrupted or contains corrupted files.Replace or repair the SD card.
- Rebooting the HMI device is required but does not solve the export issue.Insert the SD card into a computer to verify that the SD card meets requirements and follows any prompt to scan and repair the file system index on the SD card.
Provide Feedback