Alarms missing from Alarm Manager

Possible cause and solution:
  • The connection to a controller is lost or cannot be established.
    Establish a connection to the controller.
  • A controller flash update is in progress.
    Wait until the flash update to the controller is complete.
  • The controller firmware is invalid.
    Verify and modify the correct controller firmware if necessary.
  • There is low memory in a controller.
    Restart the controller manually to free up some memory.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal