Alarm data is not visible
Possible cause and solution:
- The Alarm, Event, or Communication service ends because the HMI device is out of memory.On the HMI device, open theSettingsscreen, tapHMI Device, and on theHMI Devicepopup, look at the memory use. TapRebootto manually restart the HMI device to free up memory.
- The Alarm, Event, or Communication service ends. If the Communication service terminates, alarms appear with bad quality. There is no notification if the Alarm or Event services end.If any of the services ends, the HMI device restarts automatically.
- The controller is unavailable due to an error in communication updates. The affected alarms appear as bad quality.Check the network connections. Open theSettingsscreen, tapHMI Networkand on theNetworkpopup, tap theNetwork Diagnosticstab
. - The project configuration is too large.Reconfigure the project to display the recommended limit of up to 500 alarms.
Provide Feedback