Unable to delete Add-On Graphic
Possible cause and solution:
- Instances of the Add-On Graphic exist in the project.Remove all instances of the Add-On Graphic from the project and then remove the definition of the Add-On Graphic.
Provide Feedback