Invalid configuration
Possible cause and solution:
- Binding directly to a controller tag from within the definition of an Add-On Graphic is not allowed.Create user-defined data type property to bind the Add-On Graphic to a controller tag.
- Cannot bind to an alias property from within the definition of an Add-On Graphic.Alias a property in the definition of an Add-On Graphic.
Provide Feedback