Cannot paste content
Possible cause and solution:
- Add-On Graphics cannot contain other Add-On Graphics.Add a graphic element to the definition of the Add-On Graphic instead.
- The definition of the Add-On Graphic is deleted.Pasting an instance of an Add-On Graphic is allowed only if the definition for the Add-On Graphic exists. Paste an instance of an Add-On Graphic for which a definition exists.
Provide Feedback