Cut or copy table content
Cut or copy table content within or across
View Designer
projects. Copy table rows or cells from State Tables
and Color Tables
. Copy rows from the table on the Property Definition
tab. Single cells cannot be cut.Prerequisites
- Open the sourceView Designerproject containing the content to copy.
- If the content is to be pasted into another project, for each project, start an instance ofView Designerand open the target project. Open up to three instances ofView Designerat one time.
To cut or copy table content
- Cut or copy the content:
- To cut a table row, right-click the row to cut and selectCut. Only an entire row can be cut.
- To copy a table row or cell, right-click the row or cell to copy and selectCopy. Copy a single cell or a range of cells.
- Right-click on the row or cell to paste the content and selectPaste.TIP:Tips:
- The yellow star burst
indicates a new row. - When pasting an entire row, the destination row must have the same number of columns as the source row.
- Paste content into cells that have the same type of content.
- Pasting data copied from an external program into a table is not recommended.
- Pasting data copied from a table into an external program is supported.
Provide Feedback