Rename a data log

By default, the initial data log added to a
View Designer
project is named DataLog_001. This number is incremented when creating a new data log with the same name. A project can contain up to three data logs.
Rename a data log to make the name that reflects its purpose, content, or targeted use. Names within a folder must be unique and are not case sensitive. For example, Monthly_DataLog and monthly_datalog are considered identical names.
To rename a data log
  1. In the
    Project Explorer
    , expand the
    Data Logs
    folder.
  2. Select the data log once to select the item.
  3. Select the data log again and type the new name.
    TIP:
    Tips:
    • Right-clicking a data log, selecting
      Rename
      , and entering a new name also renames the data log.
    • Change the name of the data log through the
      Name
      box in the
      Properties
      window of the data log.
    • Changing the name of the data log causes previously collected data to no longer appear in the data log when the project downloads again.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal