Corrected anomalies
This list identifies the anomalies that are corrected in the Logix Designer application
version 38.03. Use the identification information provided in parentheses to track the anomaly
in future releases or for reference when receiving assistance from Customer Support with a
related issue.
General
Axis scaling error in Windows 11 with Logix Designer (5627266, 5671236)
An error occurs when changing axis scaling parameters in Studio 5000 Logix Designer on
Windows 11. For example, changing the Scaling Position Numerator value results in error
16427-80042FD2. This error does not occur on Windows 10.
To mitigate, export the project to L5K format, edit the scaling parameters, and re-import, or
set Scaling Source to Direct Scaling Factor Entry before applying changes.
This anomaly corrected in version 38.03.
This anomaly first identified in version 32.00.
Incorrect Warning Returned when Verifying a Function Block Diagram Routine (5277044,
5355097)
When verifying a Function Block Diagram routine, where an immediate tag value is input into a
Function Block Instruction member of a smaller datatype, the following error is reported:
Using 64-bit input with FBD Blocks having 32 bit backing tag members can produce
unexpected result.
This warning appears, even if the FBD instruction member is not a 64-bit data type.
The warning should read as follows:
Using input values outside the range that FBD block members can hold could produce
unexpected results.
Immediate values are stored as a 32-bit value by default, so if they are input to any
datatype smaller than 32-bit, a warning is expected.
This anomaly corrected in version 38.03.
This anomaly first identified in version 36.00.
Fatal error 0x8004203b when uploading specific project (5593747, 5662441)
A fatal error 0x8004203b occurs when uploading a specific project
file that contained a Structured Text routine with an inline comment that was not placed on
its own dedicated line. For example, uploading the file V39_ST_Fatal_23.ACD results in a fatal
error instead of completing successfully. To resolve this, place the comment '//HYF 20250617'
on its own line in the affected project file.
This anomaly corrected in version 38.03.
This anomaly first identified in version 36.03.
Sequence Manager parameter values and descriptions are lost after project upgrade
(5803385, 5837547)
When a version 35 project containing an Equipment Sequence Diagram is upgraded to version 36,
Sequence Manager parameter values and initial values are reset to 0, and parameter
descriptions are removed.
This anomaly corrected in version 38.03.
This anomaly first identified in version 35.00.
Provide Feedback