Go to a Grid Location

To go to a specific grid location in the Function Block or SFC editor
:
  1. From the
    Go to
    what list, select
    Grid Location
    .
  2. In the
    Move to grid
    location
    box, type the coordinates of the grid location to which you wish to go to (for example, B24).
  3. Select
    Go To
    . The specified location is centered in the Editor window.
To access the Go To dialog box:
  • To access the
    Go To
    dialog box, select the right mouse button while in the Ladder Editor and select
    Go To
    . For more details, see Go To dialog box settings
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal