Danger: Scheduling programs online affect safety task

You are attempting to schedule a program or programs while the system is online by dragging them to a Safety task in the
Controller Organizer
. Scheduling programs while online changes the execution of programs and may have unintended consequences.
Select
OK
to schedule the program(s), or select
Cancel
to not schedule the program(s).
Note that you cannot do the following when online or offline:
  • Drag a standard program to a Safety task in the
    Controller Organizer
    .
  • Drag a safety program to a standard task in the
    Controller Organizer
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal