Function block display

Function block displays are transparent to enable underlying wires or blocks to show through a block positioned on top of them. Outlines of the block, parameter names, mnemonics, tag names and descriptions, and parameter values all appear in blue, by default. Text that the user enters appears in black, by default. If desired, modify these colors.
TIP:
When a connection in a Function Block diagram appears as a diagonal line, rearrange the elements to create more space in the diagram. When the connection fits in the diagram, the line changes to an orthogonal line.
Some function block instructions contain one or more special arrays. In these cases, the name of the array appears after the visible parameters. The tag assigned to the array displays next to the special array name. If no tag is assigned, the array name still appears.
Functions in the
Function Block Diagram Editor
are similar to instructions, but do not require backing tags, require less memory than instructions, sometimes execute more quickly, and use less space in a function block diagram.
TIP:
Function Block functions are available only on
CompactLogix
5380,
ControlLogix
5580,
Compact GuardLogix
5380,
GuardLogix
5580, and ControlLogix 5590 controllers
This picture illustrates how a typical function appears in a function block diagram. The two nodes on the left side of the function are inputs, and the single node on the right side is an output. Functions are labeled with a symbol rather than with text.
FBDfunction_v33
TIP:
To hide or display the value of output pins on functions or the input pins on function blocks, select
Tools > Options
to open the
Workstation Options
dialog box. Select FBD Display and select or clear
Show values of FBD Function output pins
and
Show values of input pins
. Values are displayed by default.
This picture illustrates how a typical function block instruction appears in a function block diagram.
fbd_sampleBlock_v32
This table provides examples from the instruction illustration with descriptions of the elements in the function block display:
Item
Element
Example
Description
1
Block Tag Description
ALM tag description
The description entered for this tag.
2
Instruction Mnemonic
ALM
The abbreviation for the name of the instruction, also referred to as a mnemonic, that is associated with this block.
3
Block Properties Button
...
Click this button to access the
Function Block Properties
dialog box.
It is also acceptable to press
Alt + Enter
to access the
Function Block Properties
dialog box.
4
Type Description
Alarm
The description associated with this block type.
The data type for the tag is the structure type associated with the block type. If deleting this tag from the
Tag Editor
, the
Function Block editor
considers this tag an unknown type, and a blue X appears next to the Type name indicating that the block is not verified.
5
Block Tag Name
ALM_01
The name of the tag associated with this block.
When creating the function block, the Function Block editor assigns a default tag name. To edit this name, double-click the name and choose another tag from the Tag Browser, or rename the tag on the Tag tab of the Function Block Properties dialog box.
TIP:
  • Modifying a block's tag name assigns a new tag name (that is, the previous tag is not automatically deleted).
  • The data type for the tag is the structure type associated with the block type. If this tag is deleted from the
    Tag Editor
    , the Function Block editor considers this tag as an unknown type, and a blue X appears next to the Type name to indicate that the block is not verified.
If online, start a pending edit to modify the tag name.
6
Input Parameter
In
Input parameters for the function block appear on the left side of the block.
7
Output Parameter
HHAlarm
Output parameters for the function block appear on the right side of the block.
8
Data References
In a function block routine, external tags or system values can bring in data, external tags or system values can send out data, and signals can be transmitted across routines without wiring. To do this, use:
  • Input data element references (IREF), which bring values from data elements (such as I/O data) or literals into a routine.
  • Output data element references (OREF), which send values from the routine into data elements (such as I/O data).
  • Input and output wire connectors (ICON and OCON), which provide a visual indicator of a signal's path without a wire, or where wires cannot be drawn (for example, across sheets).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal