Image column
Data grid object column that contains data represented with images.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Width | Width | Width of the element. Value greater than or equal to zero. Auto sets value to the width of the content. Absence of content collapses the element. | |
Height | Height | Height of the window. It can assume values greater than or equal to zero. The Auto value sets the height equal to the height of the content (in this case, in the absence of content the object collapses). |
Provide Feedback