Event configuration
Configuration of an event type to monitor through Events logger.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Event source | EventSource | Source node of the events of interest. If empty, considers the events of interest generated by any project object. | |
Listen subtree | MonitorSubtree | If True, sources child nodes of the node selected in Event source. | |
Non-interactive sessions excluded | ExcludeNonInteractiveSessions | Records only the events generated by user interactions with the application graphical interface and ignores events generated by other logics. |
Provide Feedback