Switch FactoryTalk Design Workbench language

Use the
Settings
page from the
File
menu to switch the language of the
FactoryTalk Design Workbench
software. The language change takes effect after restating
FactoryTalk Design Workbench
.
To switch FactoryTalk Design Workbench language
  1. From the
    File
    menu, select
    Settings
    .
  2. In
    Settings
    , on the
    General
    page, select a language from the
    Language
    list.
  3. Select
    OK
    .
  4. Restart
    FactoryTalk Design Workbench
    for the language change to take effect.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal