Update the product lifecycle information

Use the
Settings
menu to update the lifecycle status information for your device.
Prerequisites
  • Ensure connection to the network.
  • Rockwell Automation
    's website is accessible.
To update the product lifecycle information
  1. From the menu bar, select
    File
    Settings
  2. In
    Settings
    , select
    Product lifecycle
    .
  3. Select
    Update device lifecycle information
    .
    Select
    Automatically update every 90 days
    as needed.
If the update fails, the lifecycle status remains not changed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal