Rename a controller
Use the
Properties
pane to rename a controller.Naming conventions are as follows:
- The name can contain up to 32 characters.
- The name is restricted to alphanumeric characters and underscores.
- The name cannot end with an underscore or contain consecutive underscores.
To rename a controller
- InProject Organizer, select the controller.ThePropertiespane displays the controller name and catalog ID.
- In thePropertiespane, enter the new name.
Provide Feedback