Projects
A
FactoryTalk Design Workbench
project contains different components that you use to design, configure, program, visualize, and maintain your devices.A
FactoryTalk Design Workbench
project contains the following key elements:- Controller programs with the main logic for the project, executing a set of instructions
- Configuration settings for controllers, drives, I/Os, and project-specific settings
- Variables that are both global and local
- User-defined date types, including arrays, structures, and defined words
Provide Feedback