Add a user-defined function using Project Organizer
Use
Project Organizer
to add a user-defined function (UDF) to the controller project.To add a UDF using Project Organizer
- InProject Organizer, expandAssets.
- Right-clickUser-Defined Functions, and then selectNew user-defined function.
- InNew user-defined function, enter the UDF name, select the UDF type, and then enter the description as needed.
- SelectCreate.
Provide Feedback