Add a program to a project
Use
Project Organizer
to add a structured text (ST), ladder diagram (LD), or function block diagram (FBD) program to a controller project.Prerequisites
- The controller is offline.
To add a program to a project
- InProject Organizer, right-clickPrograms, and then selectNew program.
- InNew program, enter the program name, select the program type, and then enter the description as needed.TIP: The program name must be 1 to 128 characters long, starting with a letter or underscore, followed by letters, numbers, or underscores. The program name cannot contain consecutive underscores.
- SelectCreate.TIP:To rename a program, inProject Organizer, select the program, and then in theNamebox of thePropertiespane, enter the new name. Renaming a user program automatically updates all references to the program.
Provide Feedback