Add rung comments

Comments are optional for rungs in the ladder diagram (LD) language editor.
Comments are:
  • Entered above the rung.
  • Saved in rich text format.
  • Stored in the controller.
To add rung comments
  1. In the LD language editor, right-click a rung, and then select
    Add rung comment
    .
  2. In
    Rung comment
    , enter the comments.
  3. Select
    Accept
    .
    TIP: To edit or delete the rung comment, right-click the rung and then select
    Edit rung comment
    or
    Delete rung comment
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal