Add a ladder diagram branch level
Instructions placed in a branch level direct the Program Organization Unit to execute the instruction in the current branch level or the instructions in other branch levels.
To add a ladder diagram branch level
- FromToolbox, drag
to a valid location to add a parallel rung.
indicates a valid dropping location.
Provide Feedback