View instruction block parameters

In language editors, use the
Open instruction parameters
context menu to view the local variables that are assigned to the instruction block.
To view instruction block parameters
  • In the language editor, right-click the instruction block, and then select
    Open instruction parameters
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal