View instruction block logic

Open the instruction block logic to view and edit the logic, input, and output of a user-defined function (UDF) or user-defined function block (UDFB).
To view instruction block logic
  1. Open the program that contains the UDF or UDFB.
  2. Right-click the UDF or UDFB, and then select
    Open instruction logic
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal