Re-order elements in function block diagram programs
In the function block diagram (FBD) language editor, move elements to change the execution order.
To re-order elements in FBD programs
- Do one of the following:
- Drag an individual element to the new location. Connections will re-organize when the mouse is released.
- Use theCTRLorShiftkey, or drag the cursor to select several elements, and then drag the selected elements or the selection area to the new location. Connections will re-organize when the mouse is released.
Provide Feedback