Embedded communication channels

The L20E and L50E controllers have the following additional embedded communication channels:
  • A non-isolated RS-232/485 combo port
  • A non-isolated USB programming port (L50E only)
  • An RJ-45 Ethernet port
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal