Output Unlatch (OTU)
OTU enables Boolean output of a connection line Boolean state.
OTU

The associated variable is reset to FALSE when the Boolean state of the left connection becomes TRUE. The output variable keeps this value until an inverse order is made by an OTL. The state of the left connection is propagated into the right connection. The right connection must be connected to the right vertical power rail, unless you have parallel coils, where only the upper coil must be connected to the right vertical power rail.
The associated Boolean variable must be an output or be user-defined.
OTU example

Provide Feedback