Reverse Output Energize (OTO)
OTO enables a Boolean output according to the Boolean negation of a connection line state.
OTO

The associated variable is assigned with the Boolean negation of the state of the left connection. The state of the left connection is propagated into the right connection. The right connection must be connected to the right vertical power rail, unless you have parallel coils, where only the upper coil must be connected to the right vertical power rail.
The associated Boolean variable must be an output or be user-defined.
OTO example

Provide Feedback