Restore project files from the LCD module

The 2080-LCD module functions as a backup memory module for
Micro810
controllers.
Use the
Restore from the LCD module
button on the
LCD Module
configuration page to restore project files from the LCD module to the
FactoryTalk Design Workbench
project.
Prerequisites
To restore project files from the LCD module
  1. In
    Project Organizer
    , double-click the controller to open the controller application workspace.
  2. In the
    Controller
    tree, select
    LCD Module
    .
  3. On the
    LCD Module
    configuration page, select
    Restore from the LCD module
    .
  4. In
    Memory module
    , select
    Restore
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal