Back up project files to an LCD module

The 2080-LCD module functions as a backup memory module for
Micro810
controllers.
Use the
Back up to the LCD module
button on the
LCD Module
configuration page to write the user programs and function files to the LCD module. The button is available when the
Micro810
controller is in
Remote program
mode.
Prerequisites
To back up project files to an LCD module
  1. In
    Project Organizer
    , double-click the controller to open the controller application workspace.
  2. In the
    Controller
    tree, select
    LCD Module
    .
  3. On the
    LCD Module
    configuration page, select
    Back up to the LCD module
    .
  4. In
    Memory module
    , select
    Back up
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal