Detect and clear a duplicated IP address
Use the Ethernet configuration page to configure the Internet Protocol settings in the
FactoryTalk Design Workbench
project.
TIP:
- A duplicated IP address occurs when the IP address is configured manually. To avoid duplicated IP addresses, use DHCP to automatically obtain the UP address.
- When a duplicated IP address is detected, the controller ends all Ethernet communications.
- Use theDetect duplicate IP addresscheckbox to turn on or turn off duplicated IP address detection.
Prerequisites
- The controller is inRemote programmode.
To detect and clear a duplicated IP address
- InProject Organizer, double-click the controller to open the controller workspace.
- In theControllertree, selectEthernet.
- On theEthernetconfiguration page, do one of the following to clear the duplicated address error:
- If you are using IPv4
- SelectObtain IP address automatically using DHCP, or
- SelectConfigure IP address and settings, and then enter a different IP address.
- If you are using IPv6
- SelectObtain IPv6 address automatically using DHCP, or
- SelectConfigure IPv6 address and settings, and then enter a different IP address.
Provide Feedback