Export a data log

By default, when exporting a data log, all data sets included in the data log are exported to the Downloads folder with the file name
<project-name>_<controller-name>_data_log.m8a
. If a file with the same name exists, a number will be appended to the exported file.
Prerequisites
  • The data log contains one or more data sets.
To export a data log
  1. In
    Project Organizer
    , double-click the controller to open the controller workspace.
  2. In the
    Controller
    tree, select
    Data Log
    .
  3. On the
    Data Log
    configuration page, select
    Export
    .
  4. (optional) In
    Export data log configurations
    , select the export path and enter the file name as needed.
  5. Select
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal