Import a data log

Use the
Data Log
configuration page to import a data log from an M8A file on your computer. The imported data log overwrites all data sets in the controller if any.
Prerequisites
  • The controller is offline.
  • Have an M8A file for the data log.
To import a data log
  1. In
    Project Organizer
    , double-click the controller to open the controller workspace.
  2. In the
    Controller
    tree, select
    Data log
    .
  3. On the
    Data Log
    configuration page, select
    Import
    .
  4. In
    Import data log
    , select
    Browse
    .
  5. In
    Open
    , locate and select the M8A file you want to import, and then select
    Open
    .
  6. In
    Import data log
    , select
    Import
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal