Add a data set

Data sets are components of a data log. A data log records the data values of a defined set of variables in a controller project.
Prerequisites
  • The project is offline.
To add a data set
  1. In
    Project Organizer
    , double-click the controller to open the controller application workspace.
  2. In the
    Controller
    tree, select
    Data log
    .
  3. On the
    Data Log
    configuration page, select the checkbox beside the data set you want to add.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal