MicroLogix mapping export and import

Export or add MicroLogix mapping information in bulk by exporting or importing a CSV file.
The CSV file contains information on MicroLogix address associations, including the file number, variable name, data type, and MicroLogix file type. You can export or import up to 1,000 MicroLogix mapping associations.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal