Modbus mapping export and import

Export or import Modbus mapping information in bulk by exporting or importing a CSV file.
The CSV file contains information on Modbus address associations, including the variable name, data type, address, and address used. You can export or import up to 200 Modbus mapping associations. The imported Modbus mapping association will overwrite all previous associations.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal