Bit-level comments

Bit-level comments are descriptions added to explain the purposes or functionality of individual bits.
In language editors, bit-level comments are shown when you assign variables to Program Organization Unit (POU) elements. Bit-level comments apply to the following variable types, POUs, and POU elements:
  • User-defined variables
    • Variables of the INT data type
    • Multi-dimensional arrays that are of the INT data type
  • POUs and POU elements
    • Instructions, coils, and contacts in an LD
    • Global and local variables in a UDFB
    • Global and local variables in a UDF
Bit-level comments capture the changes that are made to the associated variables when performing the following actions:
  • Add, update, or delete POUs or variables.
  • Copy or paste POUs, variables, or cross instances.
  • Export or import devices or POUs.
  • Export or import global or local variables
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal